Other Parts Discussed in Thread: CC2531
Tool/software: Linux
Hello everyone:
I am new to the use of these devices (CC2531) and I hope you can help me, I will explain the problem.
I have a Zigbee network created with Xbee devices, so I need to check that the links are secure. To do this I bought the device "Wireless Zigbee CC2531 Sniffer USB Dongle", which allows to check the links in the 2.4 Ghz frequency with the FirmWare Killer Bee.
I installed Linux Kali where the Killer Bee Firmware is installed but I can not identify my device "Wireless Zigbee CC2531 Sniffer USB Dongle", I do not know if it is a problem of the linux version, or that the device is damaged, or I need to install some driver for this .
For now, when I connect the USB device, Linux does not recognize it to mount it and Killer Bee's applications do not recognize it as a valid interface.
What do I need to do in Linux so I can use the device "Wireless Zigbee CC2531 Sniffer USB Dongle"