This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630: remote control module

Part Number: CC2630
Other Parts Discussed in Thread: REMOTI, TIMAC, CC2530ZLLRC-RD

our customers want to use the zigbee remote control, the remote control is not required to access the network. There are a few questions now.
1. When the remote control broadcasts, the devices that have already entered the network can be accepted; but if some devices are not connected to the network, it cannot receive the broadcast. And we do the remote control, originally expected to be in the absence of the host, that is, the device does not enter the network, and at least can be controlled by the remote control. But because it can't be received, it can't be controlled by the remote control. Excuse me, how can I get a module that is not connected to the network or a module that is connected to the network to receive the broadcast message of the remote control (the remote control is not connected to the network)?

2. Like the door lock module, this kind of device that uses polling for power saving, how should the remote control application be more convenient?

best regards,

Steven