Other Parts Discussed in Thread: CC1352R, LAUNCHXL-CC1352R1
Hi,
I'm excited and a bit confused to see LAUNCHXLCC1352P-2 schematic. If someone can help clarify the following for me please:
There are 4 outputs/ RF interface ports -- 2.4G (P11), SubG (P12), PA (P13) -- all three marked as "DNM" for optional assembly;
and routed via RF mux/ switch (U32) out to a single SMA (J7). Given that, my questions are:
1) Is PA (pins 5 & 6) wired inside CC1352P to 2.4G and/ or SubG TX path internally? if so,how does the selection work? Please
point me to section/s explaining this in the Tech Ref Manual (I'm referring to swcu185a).
Trying to understand say for SubG operation - am I supposed to use P12 for receive and P13 for transmit?
2) Purpose/ advantage of using mux/ switch and (2.4G, SubG, PA) combined output via J7 or A1 is to have a common antenna
and be able to select RF signal chain? I imagine this switching happens automatically controlled by the stack, vs. user code
(using DIO28-30)?
If that's the case - I suppose U32, J7/A1 are optional if user plans to populate P11 and/ or P12 along with P13. Perhaps not
even populate P13 if no PA is needed (sort of like "CC1352R" mode of operation).
Please advise. Thanks for your timely attention and help.