Part Number: CC2530
Components/mac/low_level/srf04/mac_tx.c
1.2.2a compare 3.0.1
@@ -749,19 +749,10 @@ static void txComplete(uint8 status)
{
/* mark receive as inactive */
macRxActive = MAC_RX_ACTIVE_NO_ACTIVITY;
}
- /* In general, the MAC_RX_POLL is controlled by high level MAC. The flag is
- * cleared here when no ACK is pending to allow the RX to be turned off sooner
- * in order to save power.
- */
- if (status != MAC_ACK_PENDING)
- {
- macRxEnableFlags &= ~MAC_RX_POLL;
- }
-
/* turn off receive if allowed */
macRxOffRequest();
/* update transmit power in case there was a change */
macRadioUpdateTxPower();