This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538: Debug cc2538 EM over smartRF06 dev board

Part Number: CC2538

hello,

I am facing a issue when debugging cc2538 running ZNP application mounted on smartRF06 board. ZNP application is driven by host PC application over P412 UART header and  I am using IAR 8.30.1 for debugging. It turns out that program in debug mode doesn't stop at breakpoints after starting host application. Before starting host application  program hits every breakpoints as expected. While debug mode is active znp running as expected. I have set the count variables to be sure that program enters certain functions in which the breakpoints are set.

Do you have any suggestions?

Best regards