Hello!
I use the CC2630 as the end device and the CC2630 as a coordinator.
I use TI-MAC 1.5.2 Simplelink SDK.
The measuring tool is the ammeter.
the end device is configured as standby mode ,See the following figure:
1-step
when the end device first power on, Before networking,the current moves between 60uA and 1.5mA.
2-step
Then, the coordinator power on,Associated,Power consumption of the end device is shown below:
if not send RF data,the current is 54uA(200uA measuring range for the ammeter ).
3-step
the coordinator power off, the end device always power on ,Power consumption of the end device is shown below:
the current is above 700uA by little probability(20mA measuring range for the ammeter ).
4-step
the coordinator power up again, Associated again,the current is above 700uA,Why is the current not 60uA?
5-step
the end device power off and power up again,Power consumption is shown below:
if not send RF data,the current is always 270uA(20mA measuring range for the ammeter ),Why is the current not 60uA?
6-step
If I want to reduce the terminal current to 60uA, I must reburn the program.
Data_LowPower.psd
"P.nbr.RX < 64 " belong to 1-step and 2-step.
"P.nbr.RX > 65 " and "P.nbr.RX <89 " belong to 3-step.
"P.nbr.RX > 90 " belong to 4-step and 5-step.
How do I deal with this problem? It is unavoidable that the power failure of the coordinator and the current rise of the terminal equipment will affect the battery life of the product.
Looking forward to your reply.
Thank you.