This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538: CC2538 + CC2530

Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK, CC2530

Dear  All

       My device is this configuration:

       1. CC2538 is Home1.2.2a

       2. CC2530 is Z-Stack 2.5.1a

       Question :

       1. Can build network with these two device ?

       2. Can communicate between these two device ? What need to set ? 

  • If you disable Zigbee security on both, they should be able to talk to each other. If you want to use HA profile, make sure your Z-Stack 2.5.1a CC2530 enables TC LINK KEY security and use correct TC link key for Zigbee security. Then, two stacks should be no problem to talk to each other.