This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: CC2530 IEEE MAC Error

Part Number: CC2530

Hi,

CC2530 IEEE MAC address have repeated in our mass production,How to solve it?

  • That's not possible. If you try to do erase to those CC2530 with duplicate IEEE address and read IEEE address again from Flash Programmer, do you still see duplicate IEEE address?
  • user3434218,

    As YK had mentioned, this should never be possible for the long IEEE MAC address to have duplicates. I would recommend follow YK's suggestion on mass erasing those CC2530s which you have seen duplicates on. Then use something like Flash Programmer to read them again. If they are still duplicates, please post screenshots of them for further debugging.

    Best,
    Sean
  • I think same time it is is possible. I think user3434218 copy FW from one to other.. In this case i can observate starnge sitaution with MAC.