Part Number: LAUNCHXL-CC1352P
Other Parts Discussed in Thread: CC1352R, Z-STACK
Hello
Im Rohan Rasekh
Currently im using 4 CC1352R boad to build a ZIGBEE3 mesh. i have followed instruction here to establish zigbee coordinator and router and end device in a simple mesh network. now i want to do the following
1. use INSTALL CODE for the mesh. im doing the following but its not working, if im missing something please inform me
- on COORDINATOR
- doing primary steps of reset, logical_type setting
- seting PAN ID using SYS_OSAL_NV_WRITE ,ID:83 value: 0xF0C0
- setting channels primary and secondary
- adding install code using APP_CNF_BDB_ADD_INSTALLCODE, im adding IEEE addresses of other boards and the installation code(0x1111111111111111F9FC) for them
- APP_REGESTER
- APP_CNF_BDB_START_COMMISSIONING : network formation
- APP_CNF_BDB_START_COMMISSIONING : network steering
- on ROUTER
- doing primary steps of reset, logical_type setting
- seting PAN ID using SYS_OSAL_NV_WRITE ,ID:83 value: 0xF0C
- setting channels primary and secondary
- adding install code using APP_CNF_BDB_SET_ACTIVE_DEFAULT_CENTRALIZED_KEY ,installation code(0x1111111111111111F9FC) USE GLOBAL: FALSE
- APP_REGESTER
- APP_CNF_BDB_START_COMMISSIONING : network steering
on coordinator all is successful but router can not find the coordinator
Write ZCD_NV_ZDO_DIRECT_CB to 1 to receive ZDO related messag is also enabled for both
im using Z-tools 2 and Zstack3
other matter is can i save network config ,so after power reset , they now their config?
regards
RASEKH