This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: how to switch the CC2650R's protocol at the run time?

Part Number: CC2652R
Other Parts Discussed in Thread: CC2650,

I have a question about CC2650's multiprotocol.

The CC2652R device supports multiprotocols, for example, wireless 2.4-GHz MCU targeting Thread, Zigbee®, Bluetooth® 5
low energy, IEEE 802.15.4g, IPv6-enabled smart objects (6LoWPAN), Wi-SUN®, and proprietary systems.


(1) Can some of these protocols run in a time-multiplexed way? If then, how to switch between them?


(2) Or just one protocol can run only, which is decided by the corresponding firmware loaded at the factory?