This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: CC1352 RF Parameters

Part Number: CC1352P

We are using CC1352P in our design and we have the below queries with respect to RF parameters

1) Please let us know whether the minimum transmit power of the device @ 2.4 GHz for a data rate of 250Kbps is <= -3 dBm and meets IEEE 802.15.4 specs

2) The first and second harmonics power is not mentioned in the datasheet of CC1352P. Please let us know whether the harmonics power is < -41 dBm as per IEEE 802.15.4

3) Please let us know whether the spectrum PSD mask values, Constallation error values, Jamming resistance values meets the IEEE 802.15.4 specs.

4) Please let us know whether energy detect function is supported by CC1352P 

Thanks and Regards

VIshak N

  • Most of the answers to your questions are in the data sheet.

    Output power using 2.4 GHz PA is +5 dBm and has a programmable range of 26 dB. Spurious emission >1 GHz (including harmonics) is max -46 dBm at +5 dBm output power.

    CC1352P meets PSD requirements. The constellation error values (EVM) is given in the data sheet as 2% (typical). Jamming resistance values (=blocking and desensitization) is on page 24 in the data sheet.

    CC1352P has an RSSI dynamic range of 100 dB and carrier sense functionality (= energy detect function)
  • Part Number: CC1352P

    Thank you for the response

    Also let us know on the below queries

    1)  Please let us know whether the Crystal reference oscillator accuracy is within +/- 40 ppm 

    2)  What will be the power rise and fall values limit for CC1352P

    Thanks and Regards

    Vishak N

  • Hi Vishak,

    1) This is set by the crystal specifications.
    2) This is stated in the datasheet.

    Regards,
    Fredrik