Part Number: CC2652R
Other Parts Discussed in Thread: CC2530
Hi TI Team,
What is the maximum usable packet error rate for for simple send-acknowledge application which is not always active (by demand tx-rx only).
For 100 packets sent/receive between CC2530 dev kit and our cc2652 device are getting these results:
2480MHz
Distance (m) 1 10 20 30 40 12 (2 rooms) 15 (2 rooms and 1 wall)
"Main Board as a Receiver (dBm)" -49 -65 -79 -72 -73 -82 -91
Error % 1% 1% 1% 3% 7% 3% 6%
"Main Board as a Transmitter (dBm)" -54 -74 -82 -75 -88 -86 -96
Error % 1% 4% 14% 8% 25% 7% 10%
Maximum usable packet error rate?
Regards,
Walter