This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Im confused with some configuration setups that most of them are used the configuration of slip radio as the edge node iof the 6lowpan network. So I have some couple of question regarding this.
1) What are the exact differences between these 2 configurations ( configuring the edge node as the rpl border router and slip radio)?
2) If I used a slip radio configuration as the end point node, do I have to configure the rpl border router configuration in raspberry pi?