This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SIMPLELINK-CC26X2-SDK: Having a problem with ZigBee dissectors in Wireshark 2.6.6

Part Number: SIMPLELINK-CC26X2-SDK

Followed the ZigBee Light and Switch example in the Simplelink SDK.

Pipe is set up to wireshark from the Smart RF Sniffer 2,  and data is showing up. BUT the dissector for ZigBee doesn't appear to be parsing any ZigBee data.

The version of Wireshark is 2.6.6 and is the 64 bit version. and I copied the 64 bit dll's to the 2.6 folder In wireshark. Is there an issue with using the 64 bit dlls with the newer version of wireshark?