This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2652R: SimpleLink CC13x2 and CC26x2 SDK v2.40.00.xx pre-production and production releases

Part Number: CC2652R


Tool/software: TI-RTOS

HI TI Team,

According to TI, 

The SimpleLink CC13x2 and CC26x2 SDK v2.40.00.xx is a pre-production software release. It is compatible with revision E silicon of the SimpleLink CC13x2 and CC26x2 wireless MCUs. Finalized RF settings, features, and examples will be included in the production release of the software targeted for early second quarter of 2019. After the production release of the silicon and software, customers going into production will need to migrate to the most current version of the SimpleLink CC13x2 and CC26x2 SDK.

References:

http://www.ti.com/tool/download/SIMPLELINK-CC13X2-26X2-SDK#sw-whats-new-box

Question:

1.  If we are using SimpleLink CC13x2 and CC26x2 SDK v2.40.00.xx is a pre-production software now, will it be compatible with hardware production release come end of 2nd quarter 2019?

2.  If hardware production release will come only second quarter, any recommendation if want to go production before?

Regards,

Walter