Part Number: CC2531
Other Parts Discussed in Thread: Z-STACK
Hi,
I ran into a mysterious problem recently - using TI CC2531 USB dongle acing as a Zigbee coordinator. I have a device joined the network. Everything is working fine.
Then, I plugged in a Samsung Smartthings (Zigbee) Hub. After some time (a few hours it looks like), the device stopped "talking" the my Zigbee coordinator.
Through the sniffer, there is no more traffic from the device to the coordinator. So it means that the device somehow switched to a different Zigbee channel?
Based on limited testing, if I power recycle the device, it will start communicating again.
I tried using a sniffer to sniff, the coordinator is communication on channel 11. And there's lots of traffic when everything works. When the device stops communicating, even if I snoop channels 14, 15, 19, 20, 24 & 25 there is no traffic.
Anyone knows what would happen IF there are multiple coordinators in the network (I assume Samsung hub wants / is presenting itself as a coordinator)?
Thanks!