This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: Commands are discarded when sending commands to multiple end devices

Part Number: CC2530

12 ZigBee devices connected to the ZigBee coordinator.
Each works normally.
When the ZigBee Coordinator sends data to 12 end devices, only 6 will be received and the rest will be discarded.
Are there any considerations when sending commands from multiple coordinators to multiple end devices?

1. Do I have to delay when sending commands to each end device?
2. Do I need to increase the size of the network buffer used by AF_DataRequest ()? So how can you increase the size of the network buffer?