Part Number: CC2530EMK
Other Parts Discussed in Thread: CC2530, TIMAC, CC2530-CC2591EM
Hi
I am learning ZigBee using STM32F103RB(MCU) + CC2530
The board and module went through SPI communication and operated without error.
Like Init, Send Message(AF_DATA_REQUEST) or Receive Message(AF_INCOMING_MSG) ...
I used ZNP Kit pin configuration and properly worked.
MCU CC2530
NSS <-> SS (P0_4)
SCL <-> C (P0_5)
MOSI <-> MO (P0_3)
MISO <-> MI (P0_2)
RESET(GPIO) <-> RESET
MRDY(GPIO) <-> MRDY (P2_0)
SRDY(GPIO) <-> SRDY (P1_0)
CFG0 (Not Connected)
CFG1 (Not Connected)
So now I'm trying to change communication(MCU <-> CC2530) to UART
I have tried Three pin configuration(main, alt, ZNP kit) for UART But I didn't
1. So I want to know which configuration is right way (for UART)
2. And how to wire MCU and CC2530.
I try below
MCU CC2530
RX <-> TX
TX <-> RX
CTS or NC <-> RTS
RTS or GND <-> CTS
RESET(GPIO) <-> RESET
GND <-> CFG0
GND <-> CFG1
and send SYS_VERSION (FE 00 21 02 FCS)and waiting UART Rx interrupt
3. If physical interface is good, and then how to test It. Like send to CC2530 SYS_VERSION command and check Response