Other Parts Discussed in Thread: CC1352P, UNIFLASH,
Hello,
I have three CC1352P1 Launchpads. I'm using one as a coordinator, one as and end device, and one as a packet sniffer.
When I run the SmartRF Sniffer Agent (version 1.6.0) it doesn't see any of the connected devices.
After I press the "Detect Devices" button, the toolbar at the bottom shows the message "Sniffer Device(s) Not Found".
I flashed the CC1352P sniffer board successfully using UniFlash with C:\Program Files (x86)\Texas Instruments\SmartRF Tools\SmartRF Packet Sniffer 2\sniffer_fw\bin\cc1352p1lp\sniffer_fw.hex.
The TI tool xdsdfu.exe sees all three Launchpads, the output is shown here:
USB Device Firmware Upgrade Utility
Copyright (c) 2008-2018 Texas Instruments Incorporated. All rights reserved.
Scanning USB buses for supported XDS110 devices...
<<<< Device 0 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Embed with CMSIS-DAP
Version: 2.3.0.17
Manufacturer: Texas Instruments
Serial Num: L420008V
Mode: Runtime
Configuration: Standard
<<<< Device 1 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Embed with CMSIS-DAP
Version: 2.3.0.17
Manufacturer: Texas Instruments
Serial Num: L420009P
Mode: Runtime
Configuration: Standard
<<<< Device 2 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Embed with CMSIS-DAP
Version: 2.3.0.16
Manufacturer: Texas Instruments
Serial Num: L42000CA
Mode: Runtime
Configuration: Standard
Found 3 devices.
I'm attempting to use the board with serial number L420009P as my packet sniffer (the other two boards are my coordinator and end device).
All three of my CC1352P1 Launchpads have this on the back
HW Rev A
FW SDK 2.10
And all three have a CC1352P MCU rev C.
So I need to know why my Sniffer Agent cannot detect any of my Launchpads. Any help would be greatly appreciated.
Thank you,
Tim Murtaugh