This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Thermal camera project with cc2530

Other Parts Discussed in Thread: CC2530

1. How does SampleTemperatureSensor send data to SampleThermostat?
2. Can I start a zigbee network of 50 nodes with these 2 examples? Where can I configure the network?
3. How can I send data from thermal camera to coordinator by editing 2 examples above?

Thanks you!! 

  • 1. SampleTemperatureSensor calls bdb_RepChangedAttrValue to send data to SampleThermostat.

    2. You can make SampleTemperatureSensor or SampleThermostat as coordinator and change NWK_MAX_DEVICE_LIST to configure number of nodes that can join directly to coordinator. However, CC2530 coordinator might not have enough RAM/FLASH to connect directly to 50 end devices. You might need to use routers to allow 50 devices in the same network.

    3. This sounds like a proprietary format so I suppose you need to create your own custom cluster/attribute to do it.