Part Number: CC2592
Other Parts Discussed in Thread: CC2510, CC2538
Hello,
I have made a CC2592 module for integration with CC2510. I have followed TI reference design.
But I am not getting expected result.
Below is my control pin status
PA - Connected to Vcc (3.3V)
LNA - Connected to GND
HGM - Float (Not connected) as suggested in the datasheet.
For testing purpose, initially, I took two TI CC2510 module. One as Transmitter and the other one as a receiver. The transmit power is -30dBm. When I connected both of them through a coaxial cable, the RSSI reading at receiver is -30.
When I connected CC2592 in between the two, the reading is still -30 only.
I am not observing any gain in power.
Please help
Thanks
Venu