I have read some information about more than 1000 devices can be connected to Zigbee network. Does anyone have videoes about the connection? If the connection devices are less than 1000 is also okay, but need to be more than 300. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have read some information about more than 1000 devices can be connected to Zigbee network. Does anyone have videoes about the connection? If the connection devices are less than 1000 is also okay, but need to be more than 300. Thanks.
Hi,
The theoretical limit of number of devices in a centralized Zigbee network is ~65000 (each device has unique 16-bit short address). Some addresses are reserved.
Here is a video you may find relevant: https://www.linkedin.com/feed/update/urn:li:activity:6428419668016455681/
Regards,
Toby