Part Number: CC2630
Other Parts Discussed in Thread: TIMAC
I've measured the amount of time it takes between calling the function to send a broadcast IEEE 802.15.4 message using TIMAC API and having the pin associated with PA_ENABLE/RFC_GPO1 go high during the actual message transmission out of the radio (let's call it the Tx delay), and it seems only 8 discrete values of Tx delay are possible (I took many measurements and plotted them in Excel and the distribution of delay values was clear). It looks like the radio picks a delay that is a multiple of 310us at random and uses that to push messages out. Is there a way to disable this random delay functionality? I want my Tx delay to be predictable. Thanks!