Part Number: CC2592
Other Parts Discussed in Thread: CC2530
Hi folks, in ZNP the file mac_radio_defs.c has some tables in which some values are with a TBD (to be defined) comment, in a particulary way the values that under HAL_PA_LNA_CC2592 ||MAC_RUNTIME_CC2592 MACRO. This is set for many versions of ZNP, so I have filled out with the following values that are got out from cc2592 datasheet and from
the rssi offset is different form normal rssi offset with only cc2530, Are they correct?
- macRadioDefsRssiAdj: -10, -5;
- macRadioDefsSensitivityAdj: -3;
- macRadioDefsSaturationAdj: -12;