This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The maximum transmit power level of Bluetooth for Europe

Part Number: CC2652R
Other Parts Discussed in Thread: BLE-STACK

I am evaluating the CC2652R+ Sky66403 solution which can boost the output power to above 20dBm.

According to ETSI, the maximum allowed Tx power on a Bluetooth connection is +20dBm if Adaptive Frequency Hopping (AFH) is enabled, and it is +10dBm if AFH is not enabled or if AFH is enabled but less than 15 channels are available for use.

 

Besides, ETSI has EIRP and power spectral density requirements.

 

Is AFH enable in CC2652R? Could you recommend the output power level setting of Bluetooth for Europe?