Part Number: CC2652R
Hi,
I'm using the CC2652 for 802.15.4 application (2.4 GHz). Our application circuit has a measured RX sensitivity around -86 to -88 dBm. TX power is in agreement with the selected settings in Smart RF studio. In comparison, we measure sensitivity around -98 dBm on TI 2652 eval board. One of the difference is that our applicaiton circuit is using the Johanson balun from App Report SWRA572 while the TI Eval board is using a lumped element balun.
One thing to note is that the TI Eval board's RSSI level is around -106 dBm when placed in Continuous RX mode and no signal applied. Our application circuit shows an RSSI level at -99 dBm when in Continuous RX mode and no signal applied. When I remove the Johanson balun from our application circuit, RSSI decreases to -106 level. Sensitivity on our application circuit also improves with the Johanson balun removed even though we connect to one side of the CC2652's differential input.
It seems that the Johanson balun solution is causing the sensitivity problems. Could it be that it may not be optimally matched for best sensitivity performance. Our design has followed the App Report's layout recommendations. That report is from 2017, which was written before the CC2652 was available. Does that report still apply even though it is listed for CC26XX devices? Does that balun work with the CC2652 when wanting achieve the best sensitivity? Does it require match component(s) or a layout change? Is it better to use a lumped element balun?
Please let me know.
With regards
Michael