Part Number: CC2530
Hi
My customer is now testing their network with HA 1.2.2.
Network structure is one coordinator with 36 router running in one network. Definition like NWK_MAX_DEVICES keeps as original settings. So there are 6 routers works as router and others may connect to coordinator directly or from routers.
After running this network for 3 days, there are 1/5 rate that issue shows that network is still maintaining (from sniffer log, network is still existing), routers can send request out, but no ACK from coordinator, and coordinator can send data out, but no ACK from routers.
When issue shows AssocRemove can not remove device information from AssocDevicelist succefully also.
What is possible reason for this issue? And could you suggest any debug method ?
Thanks.
Best Regards,
Barbara Wu