Part Number: CC2538
I need 2-UART for our application but in pin description of datasheet is given as PA0--UART_RX, PA1---UART_TX. which pins are used for another UART. Second UART is hardware based or programmable.
I have to connect SPI and UART, If the pin numbers PA2, PA4, PA5 are for both than how can i connect with hardware. I am designing application schematic with cc2538 give me guidance for this.