This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652RB: What is main Difference between CC2652RB, CC2592 (ACTIVE) & CC2538.

Part Number: CC2652RB
Other Parts Discussed in Thread: CC2538, , CC2652R, Z-STACK, CC1352R

Hello E2E Community,

I would like to know about the main practical Advantages & disadvantage of CC2652 over CC2538 Zigbee Device.

1. Is that CC2652 capable of interfacing Zigbee Linux Gateway Application 3.0.1. by replacing CC2538. (has UART or SPI interface?)

2. Can we simultaneously use Zigbee & Wifi Stack over CC5652?.

3. How much it is compatible with CC2538?. If we suppose to replace CC2538 device with CC2652 what are the major advantages we get?

Regard's 
Shiv Patil.