Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK, CC2592
Hi
I've compiled the stack, and I got the CC2538ZNP-with-SBL talking to the Z-Tool with RTS and CTS as well as without.
However, I can not get CC2538ZNP-without-SBL talking to the Z-Tool.
I'm using SmartRF06 paired with CC2538-CC2592EM.
Here are the options that I've used:
xHAL_UART_USB
xUSB_SETUP_MAX_NUMBER_OF_INTERFACES=5
xHAL_SPI=TRUE
HAL_UART=TRUE
BDB_FINDING_BINDING_CAPABILITY_ENABLED=0
DISABLE_GREENPOWER_BASIC_PROXY
TC_LINKKEY_JOIN
ewarm
CC2538_USE_ALTERNATE_INTERRUPT_MAP=1
CC2538ZNP
ZNP_ALT
xPOWER_SAVING
FEATURE_SYSTEM_STATS
FEATURE_RESET_MACRO
ZDNWKMGR_MIN_TRANSMISSIONS=0
MT_UART_DEFAULT_OVERFLOW=FALSE
ASSERT_RESET
MAKE_CRC_SHDW
SBL_CLIENT
ZCL_READ
ZCL_DISCOVER
ZCL_WRITE
ZCL_BASIC
I've commented:
//-DHOLD_AUTO_START from znp.cfg
I've used ZNP_ALT and MT_UART_DEFAULT_OVERFLOW=FALSE and that will disable CTS and RTS, but ultimately I want CTS and RTS.
Is there something that I've missed?
Cheers
Harry