This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538: How to get the Network Related Parameters (like Tx-Rx power, Signal strength, RSSI) of the Devices added to the network.

Part Number: CC2538

Hello E2E Community,

I am working on CC2538 ZNP device along with the Zigbee linux gateway application.

I wants to get the Network related information of each device added to the network.

such as,

1. Tx-Rx power of that device.

2. Signal Strength / RSSI.

Even if there is any other parameters related to Network OR Signal strength of the Device.

Will you help me to get this done?..

Regards,

Shiv Patil.