Part Number: LAUNCHXL-CC1352P
Other Parts Discussed in Thread: CC1352P, Z-STACK, SIMPLELINK-CC13X2-26X2-SDK, , , LAUNCHXL-CC26X2R1
I have two CC1352P Launchpads. One is running the zc_light (coordinator) example and the other is running the zed_switch (end device) example. The wireless range of these boards is very poor. If I have them close together (a few inches apart) they form a network and communicate fine. If I move the end device away from the coordinator, the end device loses its parent and drops out of the network. This loss of network occurs at a distance of approximately 15 feet, line of sight. This distance is even shorter if there is a cubicle wall between the two nodes. I'm testing in my office area, which is a typical cubicle environment. The device drops out of the network if I move it to the next cubicle. I'm using an external antenna. The performance with the internal PCB antenna was even worse.
I'm running the zc_light and zed_switch examples, with no code alterations. Since they both have CC1352P processors, the power should be 20 dBm by default.
We are developing Zigbee wireless boards using the CC1352P to be used in an industrial setting. The performance of these TI devices is horrible. We are currently using XBee radios in an industrial setting with distances of 100 feet between devices, with walls between the devices made of concrete block, and they communicate with no problems.
Is there anything you can suggest to vastly improve this performance? Do you have information on what the range of these radios should be? To make matters worse, we want to use the CC1352P with an energy harvesting circuit, which means we want to use a little power as possible, thus we want the power in dBm to also be as low as possible.
My Launchpads have revision C of the CC1352P. I'm using SimpleLink CC13x2 SDK version 2.30.00.45. It includes Z-Stack 3.2.0.
Any help would be welcome. We can't use the CC1352P processor with performance like this.
Thanks,
Tim