Part Number: CC1352P
I'm attempting to implement the OAD/OTA on a new piece of hardware (not launchpad). It is failing because the BIM expects there to already be a valid Factory New image in the external flash.
Important
SimpleLink CC26x2R1, CC1352R1 and CC1352P_2 LaunchPad boards come out-of-box with BLE project zero sample app flashed. This sample application, as part of its initialization process, will create a default Factory New image into the external flash of the LaunchPad. Zigbee OTA application assumes that any Factory New image exist, as the downloaded image will be stored as the second image available (right after Factory New image). If no Factory New image exists, the OTA Client will abort the upgrade process.
Can I bypass this check? How do I get my Zigbee Factory New image into the external flash?