Part Number: CC1352P
Other Parts Discussed in Thread: Z-STACK
Tool/software: TI-RTOS
Does the CC1352P support 900 mHz zigbee?
Can I simply exclude the "FREQ_2_4G" from the predefines?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks for the quick response.
Maybe this is more of a question for a sales guy...but are there any plans to support 900mHz zigbee?
Zigbee 3.0 is currently supported in the 2.4 GHz ISM band only. We encourage you to join the Zigbee Alliance in order to share your feedback and participate in future specification development discussions as the alliance is a member driven organization.
Since the standard only supports Zigbee on the 2.4 GHz band, how are you planning to use it on the 915 MHz band?
Hi Bill,
Zigbee PRO 2017 (r22) is required core Stack/Specification for Zigbee 3.0 certification. The Zigbee Pro 2017 Specification only mentions Sub-1 GHz operation for the Smart Energy Profile, however the Zigbee 3.0 Profile is still strictly 2.4 GHz. As TER mentions, Zigbee Alliance Members can influence the features of future Zigbee Specifications (r23+) which would then be incorporated into Z-Stack.
Edit: Some points of clarification
Regards,
Ryan