Part Number: CC2538
Hi
I'm trying to get the ZNP to automatically start in case power was lost.
I've commented out the line in znp.cfg
//-DHOLD_AUTO_START
Then I've set up a network with just 1 coordinator and 1 ZED.
However after I unplug the power of the ZC for 5 seconds, I get:
<RX>10:53:17.63 COM8 SYS_RESET_RESPONSE (0x4180)
Reason: 0x00
TransportRev: 0x02
Product: 0x00
MajorRel: 0x02
MinorRel: 0x07
HwRev: 0x02
<TX>10:53:30.18 COM8 UTIL_GET_DEVICE_INFO (0x2700)
<RX>10:53:30.2 COM8 UTIL_GET_DEVICE_INFO_RESPONSE (0x6700)
Status: SUCCESS (0x0)
IEEEAddr: 0x00124B000FE9A81A
ShortAddress: 0xFFFE
DeviceType: COORDINATOR, ROUTER, END_DEVICE (0x7)
DeviceState: DEV_HOLD (0x0)
NumAssocDevices: 0x00
AssocDevicesList
So the device went back to DEV_HOLD state.
Then I have to manually send a ZB_START_REQUEST (0x2600):
<TX>11:11:46.8 COM8 ZB_START_REQUEST (0x2600)
<RX>11:11:46.97 COM8 ZB_START_REQUEST_RSP (0x6600)
<RX>11:11:46.98 COM8 ZDO_STATE_CHANGE_IND (0x45C0)
State: 9 (0x9)
Are there any other steps that I've missed to get the ZNP to auto-start?