Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
Hi,
In z-stack 1.2.2a, if we disable MT_TASK related functions, there will be linking error. Please advise how to disable them. Thanks!
|
The definition as below: COOR_VERSION=0x05050900 xFEATURE_GREEN_POWER ZTOOL_P1 HAL_UART=TRUE HAL_UART_DMA=1 xHAL_UART_ISR=2 xMT_TASK xMT_SYS_FUNC xMT_ZDO_FUNC xLCD_SUPPORTED=DEBUG |
Error info as below: Error[e16]: Segment XDATA_I (size: 0x8a align: 0) is too long for segment definition. At least 0x27 more bytes needed. The problem occurred while processing the segment placement command "-Z(XDATA)XDATA_Z,XDATA_I=_XDATA_START-_XDATA_END", where at the moment of placement the available memory ranges were "XDATA:1e9d-1eff" Reserved ranges relevant to this placement: XDATA:1-300 XSTACK XDATA:301-1e9c XDATA_Z XDATA:1e9d-1eff ?FILL2 BIT:0-7 BREG BIT:80-87 SFR_AN BIT:90-97 SFR_AN BIT:a8-af SFR_AN BIT:b8-c7 SFR_AN BIT:f8-ff SFR_AN |