This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630: TI-RTOS power consumption while in standby mode while executing Task_sleep() function

Part Number: CC2630
Other Parts Discussed in Thread: TIMAC

I measured power consumption of my CC2630 chip while running the Task_sleep function with TI-RTOS 2.11 and TI-RTOS 2.21 using the following code:

static PIN_Handle gDbgPinHandle = NULL;
static PIN_State gDbgPinState;

void SleepTaskFxn(UArg a0, UArg a1)
{
  // Toggle the LED every 5 seconds
  gDbgPinHandle = PIN_open(&gDbgPinState, DBG_PIN_TABLE);
  int flag = 0;
  while(1)
  {
    PIN_setOutputValue(gDbgPinHandle, BOARD_DBG_1, flag);

    Task_sleep(5*1000*1000 / 10);  // Sleep for 5 seconds
    flag ^= 1;
  }
}


void main()
{
  Task_Params  sleepTaskParams;
  
  Task_Params_init(&sleepTaskParams);
  sleepTaskParams.stack = sleepTaskStack;
  sleepTaskParams.stackSize = SLEEP_TASK_STACK_SIZE;
  sleepTaskParams.priority = TASK_PRIORITY_HIGH;
  Task_create(SleepTaskFxn, &sleepTaskParams, NULL);

  PIN_init(BoardGpioInitTable);

  BIOS_start();
}

The results were:
For TI-RTOS 2.11:  120uA @ 1.8V
For TI-RTOS 2.21:  2.4uA @ 1.8V

My goal is to put my board in low power state for a relatively long time to save power (preferably using Task_sleep API call), then wake up the MCU after a specific amount of time, load the TIMAC stack, and start 802.15.4 radio communication for a short period of time, then go back to sleep.  TIMAC only works with TI-RTOS 2.11, so the only thing I can do is fix whatever issue is preventing the MCU from going into standby mode the way TI-RTOS 2.21 does (saving 98% of power).  So my question is, what is preventing TI-RTOS 2.11 from achieving the same power savings in standby mode as TI-RTOS 2.21?

My hardware is a custom board using the 7x7 CC2630 chip on which I performed the above mentioned measurements.