Part Number: CC2530
Hello together,
I have a problem with the consumed current of the CC2530.
If I enter sleep mode via:
SLEEPCMD = (SLEEPCMD & ~0x03) | 0x02;
PCON = 0x01;
I have a current of 250µA - which is in my expectation too high! I would expect about 5µA.
There is no leackage current from the GPIO! The only connected components are 2 pullups on pin P2.2 and P1.4 (10kOhm)
Do I have to disable any HW inside the CC2530 by code manually, before entering the sleep mode?
For example, as default in my code the ADC is running. Do I need to disable it?
Thanks for any help!
Best regards