Part Number: CC2652R
Other Parts Discussed in Thread: Z-STACK
Hello,
I am using cc2538-cc2592 emk as ZR and ZNP. and cc2652r as ZED.
while commissioning when any device try to join the network through any ZR then ZR sends update device command with status :[0x01] standard device unsecured join. nad after update device command ..joining device will not join.
During commissioning,I face this issue quite frequently
please refer packet 1404 in below sniffer capture and also refer expanded view of the update device command.
part 1 of expanded view of update device command
part 2 of an expanded view of the update device command