This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: end device frequently losing sync with parent

Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK, , CC2590, CC2591

Hi,

We are using Zstack302, ZNP Coordinator , 1 Router and 10 End devices.

It is observed that the end devices far from the coordinator keeps going out of sync with the parent.
It rejoins the network after few minutes(1-5). These end devices also keep changing parents on rejoin.
This occurs even if the LQI through the coordinator(0-10) is lower than the LQI through the router(60-70).

What may be the reason for this behavior? How can it be minimized?