Part Number: CC2538
Hi,
As I have mentioned earlier, I am using CC2538 for a custom protocol where I need to transfer and receive data.
Does the radio of CC2538 backoff automatically whenever the channel is busy? Or I have to do it in the application layer?
I am facing this issue of not able to broadcast the data to all devices listening in a particular channel.
If two devices are transmitting at a time, then the data of one device gets lost.