Part Number: CC2530
Other Parts Discussed in Thread: CC2531, Z-STACK,
Hi,
We faced an issue while joining a node to a network.
Setup: One coordinator (running at max TX power) and zero routers
Sniffing setup: CC2531. Packet info is sent from TiWsPc to Wireshark using socket mode and is decrypted in Wireshark
ZStack version: 2.6.2
Issue:
- When the node is programmed with the FW, we can see Beacon request from the node and Beacon from the coordinator
- We can see the association request from the node and the association response from the coordinator (association status: successful)
- There is no device announce after this process and the node cannot be reached at all. The node goes back to scanning channels for potential networks to join.
NOTE: We are facing this issue only when the firmware is run on a specific node (i.e.) if the same FW is programmed onto another device, the node joins the network successfully and makes a device announce.
Network key: 00:01:02:03:04:05:06:07:08:09:0A:0B:0C:0D:0E:0F