Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK, Z-STACK-ARCHIVE
Hi team,
A customer used CC2530 to make a light based on Z-Stack Lighting 1.0.2, and he found the light could not be turned on when temperature was below zero---No output from PWM.
Experimental steps:
1.At room temperature, the light worked well
2.Put the light into fridge for a while [temperature was -5℃] and turn on the light. If the light was not in a network, it can be turned on;If the light was in a network, it can be turned on but then went off. He used the gateway to send a light-on command and repeat the command, got the same phenomenon.
PS:Power, lamp bead, and drive circuit problems have been ruled out. This issue is a batch issue.
He was confused about:
1.The light could be turned on in the low temperature condition when it was not in a network,which means the PWM worked normally before joining into a network.But if joined, PWM could not work.
2.Experiment step two shows that the light could still communicate with the gateway[receive ON/OFF command], only the PWM function was disabled[he measured the waveform via an oscilloscope].
Is there any low temperature protection in the stack and how to solve this problem? Thanks in advance.
BR,
Viki Shi