Hi,
I am currently working on implementing an application.
I'm wondering if there is any difference between sending message over the air using zstack_afDataReq_t and the given commands such as "zclGeneral_SendOnOff_CmdToggle"? If I am not mistaken, the commands use similar API to afDataReq to send message? Below is the code I'm currently using to send messages.
I'm working on implementing Cluster ID 0x0B04 ELECTRICAL_MEASUREMENT application to measure analogue value from temp sensor, is there any send message api similar to zclGeneral_sendOnOff_cmdtoggle?