Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
Hello, I wanted to write my own application to communicate with Z-Stack Linux Gateway for sending and receiving commands or data, so I added a tcp client beside three clients that already exist in the ZSGW code and are connected to the Gateway, Network Manager, and OTA servers. My client connects to my own server and receive commands from it and then sends it to ZSGW apis to run it and also sends data back to my server. But the problem that sometimes happen is that after some commands are sent to my client, the Gateway server doesn't answer to any commands anymore and also sending no data back to ZSGW. I have to reset Zigbee Servers in order to GW Server works as usual. Do you have any idea what is the problem?!