Other Parts Discussed in Thread: CC2540, CC2511, CC2531
Hi all.
I am simulating the meandered antenna given in the CC2531EMK reference design. For this, I am following the AN043 "Small size 2.4GHz PCB antenna". The antennas layout are exactly, not the matching, but it s a good start point to understand how it works.
According to AN043 the impendance at the feed point is 50 Ohms. I imported the CC2531EMK gerbers and I simulated basically two different layouts: only the antenna, antenna + trace to balun. After several simulations the feed S11 params is +0.0020 dB at 2.45GHz, (impedance is 5KOhm / 90º). I used different stackups for CC2540, CC2511, etc. but the results are always the same. Please refer to the attached images for an example.
The recommended balun is 2450BM15A0002, specially designed to match the CC2531 RF ports, which just need to see 50 Ohms at unbalanced port (antenna + track).
There is something special to consider in this design/simulation?