Other Parts Discussed in Thread: CC1352P, SIMPLELINK-CC13X2-26X2-SDK
Hi,
We have a requirement to implement wireless mesh network with the following specification:
- Expected number of nodes - 1000 nos
- Expected area - 700 to 1000 acres
- Average distance between nodes - 12 to 15 m
- Frequency of data packets - On-start, periodic, instantaneous
- No. of parameters to be send - 20
Since the no of nodes are large, we are planning to use clustering approach (20 clusters or so, each cluster is of 50 nodes each.) The coordinator node has GSM, through which the data shall be uploaded to the cloud.
Based on the above requirement, please clarify the following points:
- Which wireless mesh technology is best suited for this scenario (Like zigbee, thread, 6LoWPAN etc).
- Since we use multiple clusters, how is channel routing handled in the suggested wireless stack
- Is it possible to use this solution as a add-on card
- What are the security options supported by the suggested stack
Thank you.
Ijaz