Part Number: CC2652R
Other Parts Discussed in Thread: UNIFLASH, CC2538, FLASH-PROGRAMMER
Tool/software: Code Composer Studio
I am developing a product with ccs9.3.0 and smartrf flash programmer 2 (v1.8.1).
In addition, XDS110 is used as a debugger.
However, the two software's xds110 firmware version is different.
So, if I use them alternately, two software are always request to update xds110 firmware.
Please release smartrf flash programmer 2 with updated xds110 firmware.