This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538DK: RSSI measurement accuracy

Part Number: CC2538DK
Other Parts Discussed in Thread: CC2538, SIMPLELINK-CC13X2-26X2-SDK, Z-STACK, CC2592, CC2652P, CC1352P

Hi Team,

We have a customer inquiry regarding their plan application for CC2538DK.

They would like to perform localization via RSSI with the ZigBee protocol and found CC2538. They would like to obtain the RSSI measurement between two devices. After that, they will use these measurements to perform trilateration, where I will locate an unknown node's location between three nodes with known locations. They would like to confirm the accuracy of RSSI measurement for a maximum of 60 meters?

Can this provide accurate RSSI readings (within reason, of course, due to environmental factors and such)? Other boards tried by the customer is only accurate up to 5-meter distance between nodes. Please let me know if there are other products better for customer application if CC2538 is not possible.

Thanks!

Jonathan