Part Number: CC2538DK
Other Parts Discussed in Thread: CC2538, CC2531
I have the CC2538 DK, and I'm trying to use the packet sniffer to read RSSI values, but I'm having some issues with this.
The RSSI readings I'm getting on the packet sniffer's software is not the same as the readings on my CC2538 board.
For example, I'll be receiving -29dBm on the packet sniffer's software, but on the board it says -45dBm.
I'm just wondering how the sniffer should be positioned in relation to the CC2538 boards? Right now I have the wireless sniffer (CC2531) positioned near one of the boards, but I'm thinking this may not be right.
Also, is the RSSI value in the packets received by the sniffer the RSSI measurement between the two CC2538 boards? This is what I'm hoping to obtain. If it is not, how can I use the sniffer to obtain this value?
Thank you! :)